Connect with Trusted controllers
Trusted
controllersConnect with the physical exact et
Trusted®
controller when developing an application. While connected, the Trusted
controller executes the application in real-time mode. When connecting an application, the AADvance-Trusted SIS Workstation software
verifies the coherency between the current application definitions and the compiled code on the Trusted
controllers.A
Trusted
controller supports a maximum of one connection from a AADvance-Trusted SIS Workstation software
.Prerequisites
- Build the application code and download the code to the target.IMPORTANT: Modifications other than these to a project may affect the accuracy or availability of monitored values when connecting without rebuilding and downloading:
- Minor graphical changes not affecting the execution order
- Descriptive text such as comments, element descriptions, and diary entries
- Migration from a legacy project
- Addition to the global library of functions and function blocks not used in the project
- Addition or removal of spy lists or ISaVIEW screens
To connect an application
- In thePropertieswindow for the device, configure theHost AddressandHost Socket Portproperties.
- From theProjectmenu, selectConnect Mode>Online. TheOnlinemenu displays online command options.
- Build the project code.
- Download the project code to the physical controller.
- In theApplication View, select theProjectelement, and then selectOnline > Connect. TheAADvance-Trusted SIS Workstation softwaresaves the application state.TIP:
- While connected, perform tasks that include:
- monitor values of variables, diagnostic information, and ISaVIEW screens
- lock and unlock the I/O channels of an I/O device
- modify values of variables and cycle time
- Upon disconnecting, theAADvance-Trusted SIS Workstation softwarereturns the device to the state previous to connecting.
Provide Feedback