Ellipse

An ellipse represents items like a container that displays a changing quantity of liquid as it flows to or from another object. Define the properties for the ellipse object from the
Properties
window. For the ellipse object, define properties for
Action
,
Color
,
Displacement
,
Rotation
,
Size
,
Text
, and
Visibility
. The ellipse also has frame color and width properties.
Property
Description
Frame Color
Color for the frame of the object. Possible colors are custom, web, and system colors.
Frame Width
Width of the frame for the object. Possible values are literal values.
Define fill color for objects in the
Color
properties.
To insert an ellipse
  • From the
    Toolbox
    , drag the ellipse object into the workspace.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal