Ellipse Settings
Use the ellipse settings to specify default values for the individual object properties.
To specify the default settings for ellipse objects
- From theToolsmenu, clickOptions.
- From theOptionsdialog box, expandISaVIEWSettings, then expandISaVIEWObjectSettings, and then clickEllipseSettings.
- Specify the default values for the required properties, then clickOK.
Provide Feedback