Loading
Press Release
Recent ActivityRecent Activity

New Controllers Can Simplify Machines, Improve Safety Performance

Allen-Bradley Micro870 PLC, new flagship of Micro800 family, can be used in place of multiple micro PLCs.

Share This:

LinkedInLinkedIn
TwitterTwitter
FacebookFacebook
PrintPrint
EmailEmail
Press Release
Recent ActivityRecent Activity
New Controllers Can Simplify Machines, Improve Safety Performance
Allen-Bradley Micro870 PLC, new flagship of Micro800 family, can be used in place of multiple micro PLCs.

Share This:

LinkedInLinkedIn
TwitterTwitter
FacebookFacebook
PrintPrint
EmailEmail

Machine designers can use a new micro programmable logic controller (PLC) to help optimize the control architecture in large standalone machines or systems. The new Allen-Bradley Micro870 PLC can support smart micro applications that require up to 304 I/O points, 280 KB of memory and 20,000 program instructions.

“Designers today use several PLC sizes for their automation projects” said Yeow Keng Teh, product manager, micro controllers, Rockwell Automation. “This approach requires inventory management of the different PLC sizes and maintenance of different programs. Now designers can use the Micro870 PLC to scale their controller to their application needs. This helps simplify inventory management, especially for those designing multiple machine types.”

The Micro870 PLC uses a flexible design concept that provides designers up to three plug-ins and eight expansion I/O modules. This capability allows them to easily customize or expand the controller to meet each machine type’s unique requirements.

The controller’s 280 KB memory capacity supports modular programming and the use of user-defined function blocks to help reduce design time. Additionally, machine builders can use this memory capacity to maintain a single program for all machine models that use the Micro870 PLC.

The controller communicates via EtherNet/IP and includes multiple embedded communications options, including a USB programming port, a non-isolated serial port and an Ethernet port. It can also support up to two axes of motion.

The new Connected Components Workbench software version 11 provides a single design environment for programming the Micro870 PLC. The software can also be used to configure Allen-Bradley PanelView 800 graphic terminals, PowerFlex AC drives, Kinetix component servo drives, electronic overload relays, light curtains and configurable safety relays. This feature can save engineers time and costs compared with using another programming tool for each device in a system.

A new conversion tool in version 11 makes it easier for MicroLogix customers to upgrade to the Micro800 controller family. In addition, version 11 allows Encompass members of the PartnerNetwork program to help ease configuration of complementary third-party products via graphical configuration profiles. These profiles support the Micro800 plug-ins as well as expansion I/O to help make the configuration process faster and more accurate.

Published May 31, 2018


Susanne Bergmann
Susanne Bergmann
Field Marketer, Germany, Rockwell Automation
Connect:
EmailEmail
Zhongjie Li
Zhongjie Li
Competency Center Manager, Rockwell Automation
Connect:
EmailEmail
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  • Sales
  • Customer Care
  • TechConnect Support
  • General Questions
  1. Chevron LeftChevron Left Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Press Releases Chevron RightChevron Right