Preface
This manual describes safety considerations for
ControlLogix®
5590 controllers, which are type-approved and certified for use in safety applications. Use this manual for the development, operation, and maintenance of safety components that use the
Studio 5000 Logix Designer®
application. Read and understand the safety concepts and the requirements in this manual and familiarize yourself with applicable standards, such as IEC 61508, IEC 62061, IEC 61511, and ISO 13849-1Provide Feedback