Disable the Controller USB Port
With the
Studio 5000 Logix Designer®
application, you can use a CIP™
Generic MSG with a Path of THIS to execute this option.- Add an MSG instruction to your program.This message only has to execute once, it does not need to execute with every program scan.IMPORTANT:You cannot add an MSG instruction to your program if the controller switch is in Run mode, or if theFactoryTalk® Securitysettings deny this editing option.
- Configure the Configuration tab on the Message Configuration dialog box as described in the table below.
IMPORTANT:These values are stored to non-volatile controller memory in such a way that the MSG instruction is not required to execute up each time the controller powers up.Disable the USB PortFieldDescriptionMessage TypeCIP GenericService TypeSet Attribute SingleInstance1Class33aAttribute4Source ElementController tag of SINT data type.In this example, the Source Element is named Port_Configuration.Source Length1 - Configure the Communication tab to use a Path of THIS.IMPORTANT:Messages to THIS must be unconnected messages.

Provide Feedback