Methods to Set the IP Address
The controller supports the following methods to change the IP address:
- BootP/DHCP EtherNet/IP Commissioning Tool
- FactoryTalk® Linxsoftware
- Studio 5000 Logix Designer®application
For more information on how to use these methods, see the
EtherNet/IP™
Network Device User Manual, publication ENET-UM006.
IMPORTANT:
The
EtherNet/IP™
mode in which the controller operates affects the setting and use of IP addresses on the controller. For example, if the controller operates in Dual-IP mode, you must set an IP address for each controller Ethernet port. That is, you must complete the steps that are described in this section twice–once for each port.Provide Feedback