Settings that Do Not Affect the Safety Signature
    In the Logix Designer application, version 36 or later, you can make the following changes to a safety project with no effect on the safety signature:
- Change the controller slot number, if applicable.
 - Modify controller IP settings.
 - Change theEtherNet/IP™mode on a controller that support multiple modes.To change theEtherNet/IP™mode, you must first delete the safety signature. After changing the mode, you can regenerate the safety signature with the same value.
 
Provide Feedback