History of Changes
    This appendix contains the new or updated information for each revision of this publication. These lists include substantive updates only and are not intended to reflect all changes. Translated versions are not always available for each revision.
Change  | 
|---|
Added information about choosing an automatic configuration setting  | 
Added security certification information to Commissioning Lifecycle section  | 
Added important information to Download the Safety Application Program section  | 
Added Restricted Access to Safety Lock/Unlock section  | 
Revised the  GuardLogix®  system checklist | 
Change  | 
|---|
Added catalog numbers 1756-L81ESXT, 1756-L82ESXT, 1756-L83ESXT, 1756-L84ESXT, and 1756-L8SPXT  | 
Added security certification information to Commissioning Lifecycle section  | 
Corrected maximum application rating for Safety Add-On Instructions  | 
Updated temperature in the footnote of the Safety Parameters table to reflect GuardLogix-XT™  range | 
Change  | 
|---|
Added new chapter about the safety signature: Chapter 2, Safety Signature  | 
Added catalog number 1756-L85ES  | 
Updated text and screen shot for I/O replacement options  | 
Added new section, Safety Signatures Elements, to Chapter 6  | 
Added Safety Signature Report to safety revalidation considerations  | 
Added requirement to initialize safety critical AOI tag values in AOI prescan logic  | 
Updated safety instructions throughout Appendix A  | 
Added information about the safety signature element for AOIs  | 
Change  | 
|---|
Added  GuardLogix-XT™  catalog numbers | 
Revised  Compact GuardLogix®  5380 SIL 3 Controllers section in Chapter 2 | 
Moved Use of Human Interfaces section from Chapter 5 to Chapter 2  | 
Added SIL 2 and SIL 3 Considerations for Safety I/O Modules section to Chapter 3  | 
Moved Differentiate Between Standard and Safety section from Chapter 5 to 1756-UM543  | 
Added Safety Programs, Safety Routines, and Safety Tags sections to Chapter 5  | 
Added safety mapped tags  | 
Revised safety signature content  | 
Revised Generate the Safety Signature section in Chapter 6  | 
Revised Lock the Controller section in Chapter 6  | 
Added Safety Programming Considerations chapter  | 
Added First Scan Safety Tag Initialization section to Chapter 7  | 
Added Develop a Fault Routine section to Chapter 8  | 
Moved safety fault codes from Chapter 8 to 1756-RD001  | 
Added Use GSV/SSV Instructions in a Safety Application section to Chapter 8  | 
Added ATAN2 safety instruction  | 
Added information about connection reaction time limit  | 
Added checklist item for  GuardLogix®  system | 
Change  | 
|---|
Restructured and updated the Additional Resources table  | 
Updated  GuardLogix®  5580 controllers and safety partner in chassis illustration | 
Added content about on-delay and off-delay functions for input signals  | 
Added content about the safety I/O configuration signature  | 
Added content about electronic keying implications for safety I/O device replacement  | 
Added new section about point operation types  | 
Added new section about safety I/O configuration variations  | 
Added considerations for assigning safety network numbers (SNNs)  | 
Added content about tag mapping  | 
Added content to safety application status table  | 
Added new section about revalidation considerations for the commissioning lifecycle  | 
Revised content about inhibiting a device  | 
Change  | 
|---|
Clarified safety signature information  | 
Added safety signature ID definition  | 
Change  | 
|---|
Added  Compact GuardLogix®  5380 SIL 3 controllers information | 
Updated text in the Differentiate Between Standard and Safety section  | 
Updated text in the SIL 2 and SIL 3 Safety Application Differences section  | 
Provide Feedback