Safety Network Numbers (SNNs)
    Communication within a control system travels over subnets that are interconnected with bridging or routing components. The following are examples of subnets:
- The backplane of a chassis
 - A bank of I/O modules
 - An Ethernet subnet within a LAN
 
Rather than creating a UNID directly for each 
CIP Safety™
 device, which can be prone to error in a large system, each subnet has a unique safety network number (SNN), and the UNID is created from the SNN + the node address. Provide Feedback