Checklist to Develop a Safety Application Program
    Use the following checklist to help maintain safety when you create or modify a safety application program.
✔  | System Requirements  | 
|---|---|
Are you using version 31 or later of the  Studio 5000 Logix Designer®  application? | |
Were the programming guidelines followed during the creation of the safety application program?  | |
Does the safety application program contain only a ladder diagram?  | |
Does the safety application program contain only safety instructions?  | |
Does the safety application program clearly differentiate between safety and standard tags?  | |
Are only safety tags used for safety routines?  | |
Have you verified that safety routines do not attempt to read from or write to standard tags?  | |
Have you verified that no safety tags are aliased to standard tags and vice versa?  | |
Is each safety output tag correctly configured and connected to a physical output channel?  | |
Have you verified that all mapped tags have been conditioned in safety application logic?  | |
Have you defined the process parameters that the fault routines monitor?  | |
Have you sealed any safety Add-On Instructions with an instruction signature and recorded the safety instruction signature? Optional for one time use Add-On Instructions. Required Add-On Instructions are reused on different applications.  | |
Did you measure potential alarm bursts during system commissioning and change the project if measured scan times are not acceptable?  | |
Has an independent safety reviewer reviewed the program, if necessary?  | |
Has the review been documented and signed?  | 
Provide Feedback