At powerup, the adapter reads the rotary switches to determine if they are set to a valid number for the last octet of the IP address. If the settings are a valid number, these conditions result:
  • IP address = 192.168.1.xxx (where xxx represents the switch settings)
  • Subnet mask = 255.255.255.0
  • Gateway address = 0.0.0.0
  • The adapter does not have an assigned host name, nor does it use any Domain Name System
  • If the network does not use 192.168.1.x, do not change the switch positions before you install the adapter. After you install and power up the adapter, you can use the following to set the network IP address:
    • DHCP server
    • BOOTP DHCP EtherNet/IP Commissioning Tool
    • FactoryTalk® Linx
To reset the adapter to its initial out-of-the-box settings, set the rotary switches to 888 and cycle power.
For more information on how to use software to set the IP address, see the EtherNet/IP Network Devices User Manual, publication ENET-UM006.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal