Print screen to PDF
The functionality allows you to capture the view of the screen and save it in a PDF
format.
- In thePropertiessection, navigate to theEventstab.
- From theAdd Eventdrop-down menu, select an event.
- From theAdd commanddrop-down menu, select .
- Complete the following parameters:
- FileName: Name your filePrintScreen
- ConflictResolution: If your file has the same name as the file that already exists on the server, you can choose if you want to overwrite the existing file, rename it (if you choose this option, the renamed file will have the suffix _001, _002, etc.), or skip the file that has the same name.
- Destination: Select a USB or SD card as the screen capture destination.
- Status: Statuses change during the process:
- 0 - Initial
- 10 - Successful
- 20 - In progress
- 30 - Missing or wrong command attribute
- 40 - Media not available
- 50 - Existing file
- 60 - Unexpected error
TIP: Using the status parameter allows you to follow the process.
Provide Feedback