Restrict access to the HMI device

Restrict access to the HMI device by selecting a method for users to log on to the HMI device:
To restrict access to the HMI device
  1. On the
    Project > Project Properties > Log On Method
    tab, select a Security option:
    • Use user name/password for logging on
    • Use PIN for logging on
  2. On the
    Tools > Security Administration > Users
    tab, enter a password or PIN for each user.
  3. (optional) On the
    Security Administration > Policies
    tab, adjust the complexity requirements for passwords by specifying
    Password Policy Settings
    :
    • Log off the user after a period of inactivity.
      Set in minutes how long the user has to remain inactive to be automatically logged out.
    • Minimum password length
      . Specify the minimum amount of characters required. The maximum number allowed is 14.
    • Password history
      . Type the number of previous passwords to remember. This enforces a password history and sets how frequently you can reuse old passwords. The maximum number allowed is 24.
    • To disable this feature, set the
      Number of Passwords to Remember
      to zero.
    • Passwords must meet complexity requirements.
      Select this option to enforce complexity requirements when you create or change passwords.
      TIP:
      Passwords that meet complexity requirements must:
      • Not contain the User Name.
      • Not contain any portion of the Full Name.
      • Contain characters from three of four categories:
        • Uppercase characters of European languages (A through Z, with diacritic marks, Greek and Cyrillic characters)
        • Lowercase characters of European languages (a through z, sharp-s, with diacritic marks, Greek and Cyrillic characters)
        • Numbers 0 through 9
      Non-alphanumeric characters ~!@#$%^&*_-+=`|\(){}[]:;"'<>,.?/

Password information

When you choose a password that has 100 or more characters, everything that is more than 100 will be cut and the system will not return an error message.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal