Add ports to open ports list

Add ports to the list of open ports to allow the HMI device to communicate with devices and web services that use specific ports. Add a maximum of 1000 ports.
To add ports to the list of open ports
  1. Select
    Tools > Security Administration
    and select the
    Ports
    tab.
  2. Select AddIcon
    Add ports to open
    . The focus automatically moves to the new list row.
  3. Enter a port number (1-65535) in the
    Port
    list.
  4. Select
    OK
    to save the changes and close the
    Security Administration
    window,
    or select AddIcon
    Add ports to open
    to continue adding ports.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal