Enable a data log

You can enable a previously disabled data log. By default, data logs are enabled.
Create an event to trigger the command:
    • Touch press.
      Occurs when touching the item on the screen that is configured with the event.
    • Touch release.
      Occurs when releasing the item on the screen that is configured with the event.
    • Key press.
      Occurs when pressing the specified key.
    • Key release.
      Occurs when releasing the specified key.
  1. Select the graphic element configured with the touch or key event.
  2. In the
    Properties
    pane, navigate to the
    Properties
    tab.
  3. In the
    General
    section, next to
    Text
    , provide a name of the command, for example Enable Data Log.
  4. Navigate to the
    Events
    tab and from the
    Add Command
    drop-down menu expand
    Data Log
    .
  5. Select
    Enable Data Log
    .
  6. In the
    Enable Data Log
    section, from the drop-down menu, select the data log you want to disable.
    TIP: You can enable logs separately or disable all logs.
The data log status changes to 10. See Add a Status tag to a data log.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal