Disable a data log
Disable a data log when you want to temporarily stop logging data for a
tag.
TIP:
The data log service runs even if all data logs are
disabled, and the status of
Data Logger
on the Data
Export
settings screen is 'Running'.Create an event to trigger the command:
- Touch press.Occurs when touching the item on the screen that is configured with the event.
- Touch release.Occurs when releasing the item on the screen that is configured with the event.
- Key press.Occurs when pressing the specified key.
- Key release.Occurs when releasing the specified key.
- Select the graphic element configured with the touch or key event.
- In thePropertiespane, navigate to thePropertiestab.
- In theGeneralsection, next toText, provide a name of the command, for example Disable Data Log.
- Navigate to theEventstab and from theAdd Commanddrop-down menu expandData Log.
- SelectDisable Data Log.
- In theDisable Data Logsection, from the drop-down menu, select the data log you want to disable.TIP: You can disable logs separately or disable all logs.
The data log status changes to 20. See Add a Status tag to a data log.
Provide Feedback