Export a View Designer project
Export a
View Designer
project as a set of files. You can import the exported files to another View Designer
project, and you can use any text editor to modify the project. Network paths and Sharepoint are not supported, but you can use drive mapping. For more information, see Best practices and limitations.- With the project open inStudio 5000 View Designer, from the menu bar, selectFile > Export Project.
- In theExport projectwindow, enter or browse to the location where you want to export the project.TIP:Namecontains the name of the project as it appears inView Designer.
- SelectExport. When export finishes successfully, a prompt appears.
- To open the location of the exported content, select the link to the file path. The location contains a folder with the same name as the exportedView Designerproject.
- Use a text editor to open any exported file and view or edit the content.
Provide Feedback