Format of ViewApplication.hmi file
The ViewApplication.hmi is a text file that contains the settings of a specific exported
View Designer
project. The .hmi file follows the structure:
namespace ViewDesigner;
using HMICatalog;
ViewProject [name] {
<homescreen declaration>
}
For example:
namespace ViewDesigner;
using HMICatalog;
/* HMI Device Type: 15" PanelView 5510 2715P-T15CD */
ViewProject SampleProject{
HomeScreen := "Screen_001";
}
Provide Feedback