Navigation Menu syntax

The navigation menu exports as a set of folders and .hmi files matching the structure of the navigation menu configured for your project. The .hmi files represent the shortcuts you configured in your navigation menu.
Shortcut .hmi files follow the structure:
namespace ViewDesigner;
using HMICatalog;
/* HMI Device Type: 9" PanelView 5510 2715P-T9WD */
Shortcut [name] (
<screen property bindings>)
{
<shortcut property definitions>
}
For example:
namespace ViewDesigner;
using HMICatalog;
/* HMI Device Type: 9" PanelView 5510 2715P-T9WD */
Shortcut Mixer1Detail (
MixerTag := "::LGX.Mixer1")
{
TargetScreenName := "User-Defined Screens\MixerDetail";
UseScreenSecurity := true;
Caption := "Mixer1
Detail";
}
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal