Contents of an exported VD project

An exported project is saved in a new folder in a specified directory.
A text file named
ViewApplication.hmi
contains project settings and is the starting point when performing import.
View Designer
exports content for screens, popups, and the graphic elements on a screen or popup into specific text .hmi files, which model aspects of visualization in the
View Designer
. The .hmi files are stored in separate folders, and the exported project folder structure corresponds to the folder structure in the
Project Explorer
in
View Designer
.
Import_Export_Content
For detailed information about the
View Designer
object properties, refer to the Studio 5000™ View Designer Help.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal