Download a runtime application to an HMI device

Use the
Download Runtime Application
wizard to transfer a runtime application to an HMI device.
IMPORTANT:
When downloading a project or flashing an HMI device that has the screen saver running, the progress may not be visible. Stop the screen saver on the HMI device before beginning the download or flash process.
Prerequisites
  • Open the project to download to the HMI device.
To download a project to the HMI device
  1. Select
    Communications > Download
    to open the
    Download Runtime Application
    wizard.
  2. Next to the
    Location
    box on the
    HMI Device Location
    page, select
    Browse
    ST5K_Project_Properties_Browse_button.jpg and select the IP address of the HMI device to download the runtime application. Select the IP address in the
    Location
    box. The
    Location
    box lists up to five previously used download locations.
  3. (optional) If the project contains multiple languages, in the
    Language
    box, select the language to display in the project.
    TIP:
    If the translated string for the download language is also blank,
    View Designer
    defaults to the language used for designing the project.
  4. Select
    Next
    .
  5. On the
    Controller References
    page:
    • Verify the information is correct. If changes are required, exit the wizard. Make the necessary changes on the
      References
      tab (
      Project
      >
      Project Properties
      >
      References
      ).
  6. Verify the controllers are synchronized. The controller icon on the
    References
    tab of the
    Project Properties
    dialog box indicates the synchronization state of the controller. The Icon: View Designer Sync Icon icon indicates that the controller is synchronizing.
    TIP:
    When starting the download process while the
    Logix Designer
    project is synchronizing with the
    View Designer
    project, the download process remains in the Building the runtime application process until synchronization is complete. This can take several minutes for a large controller application.
  7. Select
    Download
    to start the download process. The
    Download
    page
    • shows the progress of the download process as
      View Designer
      saves and verifies the project, builds the runtime application, connects to the HMI device, and transfers the runtime application to the HMI device.
If
View Designer
encounters a problem, an error message appears and the process stops. When
View Designer
finds invalid tags or expressions during project verification, the
Errors
window opens to list the warnings or errors associated with the tags or expressions. Resolve all errors before downloading the runtime application to the HMI device again.
TIP:
If a project contains a data log, and there is no change to the configuration of the data log, previously collected data remains in the data log when the project downloads again.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal