Create an HMIBC Button

Create a high-speed HMIBC button in an HMI project to initiate machine control operations, such as jogging a motor, with a high-degree of precision and determinism.
Any graphic element can be configured to function as a high-speed HMIBC button. Each Logix controller can support up to 256 HMIBC tags.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal