Change the HMI device of a project

Change the type of HMI device for a project to change the device for which the project is configured. Do this to view the runtime application on the different HMI device.
To change the HMI device of a project
  1. Select
    Project > Project Properties
    . The
    Target HMI Device
    dialog box opens.
  2. Select the HMI device. To search for the HMI device, start typing the name of the HMI device in the
    Search
    box.
  3. Click
    Next
    .
  4. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal