Add an event command to reboot the HMI device

Add an event command to reboot the HMI device. Rebooting the HMI device is also performed through the Settings screen on the HMI device.
Prerequisites
Create an event to trigger the command:
  • Touch press.
    Occurs when touching the item on the screen that is configured with the event.
  • Touch release.
    Occurs when releasing the item on the screen that is configured with the event.
  • Key press.
    Occurs when pressing the specified key.
  • Key release.
    Occurs when releasing the specified key.
  • Button behavior
    Occurs when releasing the button.
  • Project event
    Occurs when the executing condition is met.
To add an event command to reboot the HMI device
  1. Select the graphic element configured with the touch or key event.
  2. In the
    Properties
    pane on the
    Events
    tab, select
    Add Command
    .
  3. Expand the
    HMI Device Configuration
    category and select
    Reboot Terminal
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal