Add an event command to import a certificate
Import a certificate to allow encrypted communication between the web browser on the HMI device and a remote server.
TIP:
When creating a self-signed certificate, verify that the
Subject Alternative Name
property of the certificate contains the IP address of the device or server that you are connecting to.Prerequisites
Create an event to trigger the command:
- Touch press.Occurs when touching the item on the screen that is configured with the event.
- Touch release.Occurs when releasing the item on the screen that is configured with the event.
- Key press.Occurs when pressing the specified key.
- Key release.Occurs when releasing the specified key.
- Button behaviorOccurs when releasing the button.
- Project eventOccurs when the executing condition is met.
- Select the graphic element configured with the touch or key event.
- In thePropertiespane on theEventstab, selectAdd Command.
- Expand theCertificatecommand category and selectImport Certificate.
- UnderImport Certificateon the command card, in theSourcebox, selectUSBorSD Card.
- In theFileNamebox, type the file name of the certificate or or create a binding to a string which contains the file name of the certificate.
Provide Feedback