Add an event command to delete a certificate

Delete a certificate to no longer store the certificate on the HMI device.
Prerequisites
Create an event to trigger the command:
  • Touch press.
    Occurs when touching the item on the screen that is configured with the event.
  • Touch release.
    Occurs when releasing the item on the screen that is configured with the event.
  • Key press.
    Occurs when pressing the specified key.
  • Key release.
    Occurs when releasing the specified key.
  • Button behavior
    Occurs when releasing the button.
  • Project event
    Occurs when the executing condition is met.
To add an event command to delete a certificate
  1. Select the graphic element configured with the touch or key event.
  2. In the
    Properties
    pane on the
    Events
    tab, select
    Add Command
    .
  3. Expand the
    Certificate
    command category and select
    Delete Certificate
    .
  4. In the
    Fingerprint
    box, type the fingerprint of the certificate or create a binding to a string containing the fingerprint of the certificate.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal