Add an event command for navigation on the HMI device
Add an event command to navigate a screen or popup on the HMI device. Do this to open a screen, navigate screen history, open or close a popup, or open the Navigation menu on the HMI device.
Prerequisites
Create an event to trigger the command:
- Touch press.Occurs when touching the item on the screen that is configured with the event.
- Touch release.Occurs when releasing the item on the screen that is configured with the event.
- Key press.Occurs when pressing the specified key.
- Key release.Occurs when releasing the specified key.
- Button behaviorOccurs when releasing the button.
- Project eventOccurs when the executing condition is met.
- Select the graphic element configured with the touch or key event.
- In thePropertiespane on theEventstab, selectAdd Command.
- Expand theNavigationcategory and select the command:
- Navigate Backward.Navigates back in history to the screen opened using theNavigationmenu or aScreen Navigatecommand.
- Navigate Forward.Navigates forward in history to the screen opened using theNavigationmenu or aScreen Navigatecommand.TIP:Logging off the HMI device erases the navigation history.
- Show Navigation Menu.Opens theNavigationmenu on the HMI device screen when the event occurs.
- Popup Close.Closes the popup on the HMI device when the event occurs. Only one popup at a time can open on the HMI device.
- Popup Open.In theOpen Popupbox, navigate to and select the popup the event is to open. You can now select a position of a popup. See Position a popup.
- Screen Navigate.Opens the specified screen when the event occurs. In theNavigate Tobox, select the shortcut or screen that the event is to open.TIP:Tips:
- If the selected screen or popup for a Screen Navigate or Popup Open command has a user-defined data type property, bind the value in theProperty Configurationbox to the user-defined data type property of the shortcut or popup. This passes the value to the screen or popup when it opens on the HMI device.
- If a graphic element on the screen or popup to open for a Screen Navigate or Popup Open command has an aliased property with a value, the Screen Navigate command or Popup Open command can read the value from a referenced graphic element and apply it to the alias. In theProperty Configurationbox at the bottom of the command, enter the name of the graphic element and the property that has the value to apply to the aliased property. Use the format ElementName.PropertyName. When the event triggers, the graphic element on the screen or popup with the aliased property shows the property value of the graphic element that is referenced in theProperty Configurationbox. TheProperty Configurationbox appears for the command only if there is an aliased property or user-defined property on the target screen or popup.
Provide Feedback