Add an event command to interact with a PDF graphic element
Create an event to navigate pages or change the view in a PDF document. Add a PDF navigation command to a touch or key event to navigate to the previous page, next page, or a specific page in a PDF.
Prerequisites
Create an event to trigger the command:
- Touch press.Occurs when touching the item on the screen that is configured with the event.
- Touch release.Occurs when releasing the item on the screen that is configured with the event.
- Key press.Occurs when pressing the specified key.
- Key release.Occurs when releasing the specified key.
- Button behaviorOccurs when releasing the button.
- Project eventOccurs when the executing condition is met.
- Select the graphic element configured with the touch or key event.
- In thePropertiespane on theEventstab, selectAdd Command.
- Expand thePDFcategory and select and configure the command:
- Next Page. Navigates to the next page in the PDF when the event triggers.
- Previous Page.Navigates to the previous page in the PDF when the event triggers.
- Go to Page. Navigates to the specified page in the PDF. In thePagebox, enter the page number to display when the event triggers.
- Zoom In. Increases the document magnification by a percentage of the preset level in a PDF document. In theByPercentbox, enter a value to increase magnification.
- Zoom Out. Decreases the document magnification by a percentage of the preset level in a PDF document. In theByPercentbox, enter a value to decrease magnification.
- Zoom To. Adjusts the magnification of the PDF to fit an entire page, fit the width of the page, or show the page at 100% in the PDF Viewer. In theZoomlist, select a magnification option.TIP:Tips:
- Bind a PDF command property value to a tag in a controller to change the PDF property dynamically on the HMI device. If there is a problem with a tank, bind the specific page number of the PDF document to a tag for user assistance. The controller opens the document to the specified page explaining how to fix the issue.
- Project events do not support PDF commands.
Provide Feedback