Text Input
The Text Input graphic element is a control with built-in animation properties to show a string tag value and open the virtual keyboard to change the value. Text Input appears under
CommonControls
in the Toolbox.Use the Text Input graphic element to show messages from the data source on the HMI device,
and write a new value to the data source. The
Virtual Standard Keyboard
opens in PanelView
projects when interacting with a Text Input graphic element. Make the value you enter by selecting the
MaskedValue
box in the Properties
window. For example, select MaskedValue
to have users not see their passwords while they type them. Bind the
Text
box in the Properties
window to a string tag, a numeric tag, or an expression to display information from the data source. Write a new value to the tag on the HMI device using the virtual keyboard. If you enter an invalid value, the value does not write to the tag and an error appears. For example, if the Text
property is bound to an INT tag, writing the value "abc" to the tag is not supported.
TIP:
Tips:
- Do not place text against the border of a graphic element. Allow for a small difference in space, such as one or two characters. If placing text against the border of a graphic element, the text may wrap differently or appear clipped on the HMI device.
- The maximum length of a text input is 82 characters.
Built-in animation properties
Built-in animation properties appear under the
General
category of the Properties
window. Specify values for these properties in order to animate the graphic element or change the information the graphic element shows on the HMI device.Property | Category | Purpose | Accepted Values |
|---|---|---|---|
Text | General | Specifies the text on the graphic element. Do not place text against the border of a graphic element. Allow for a small
difference in space, such as one or two characters. If you place text against the
border of a graphic element, the text may wrap differently or appear clipped on
the HMI device. | Alpha-numeric characters |
Unique properties
Unique properties are properties that not all graphic elements in the
Toolbox
share.Property | Category | Purpose | Accepted Values |
|---|---|---|---|
CornerRadius | Appearance | Specifies the curve of the corners. | 0 or a positive number |
FillColor | Appearance | Specifies the fill color. | Any selected color in the Color Picker or a Hex color value entered
manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits
from 0 through F and represent the color channel values for red, green, and blue.
For example, #ffff00 produces yellow. |
TextAlignment | Appearance | Specifies the vertical and horizontal alignment of the text. | Vertical alignment:
|
Color | Appearance/Border | Specifies the color of the border. | Any selected color in the Color Picker or a Hex color value entered
manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits
from 0 through F and represent the color channel values for red, green, and blue.
For example, #ffff00 produces yellow. |
Style | Appearance/Border | Specifies the style of the border line. |
|
Width | Appearance/Border | Specifies the width of the border line. |
|
FontName | Appearance | Specifies the font of the text. | Any selected font |
FontColor | Appearance | Specifies the color of the text. | Any selected color in the Color Picker or a Hex color value entered
manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits
from 0 through F and represent the color channel values for red, green, and blue.
For example, #ffff00 produces yellow. |
FontSize | Appearance | Specifies the size of the text. | Positive numbers |
Bold | Appearance | Makes the text or value on the graphic element bold. |
|
Padding | Appearance | Specifies the distance, in points, between the content of the element and the
edge of the element. | Any numeric value |
UsePredefinedDisabled | Appearance | Specifies if a crosshatch overlay shows on the control element when you disable
the element. |
|
MaskedValue | Input | Specifies that asterisks mask the value entered on the numeric keypad. |
|
KeypadMinValue | Input | Specifies the minimum value to show and enter on the numeric keypad | Any numeric value that is less than the KeypadMaxValue property value |
KeypadMaxValue | Input | Specifies the maximum value to show and enter on the numeric keypad. | Any numeric value that is greater than the KeypadMinValue property value |
Common properties
Common properties exist for all graphic elements.
Property | Category | Purpose | Accepted Values |
|---|---|---|---|
Access | Security | Specifies if all users have access to the control element, or if access is inherited from the screen. |
|
Angle | Position and Size | Specifies the rotation angle. Enter 180 to display the graphic element upside down. If you enter a value larger than 360, the portion of numeric value that is over 360 becomes the value. For example, enter 380 to see a value of 20. If you enter a value less than 0, the negative value is subtracted from 360. For example, enter -30 to see a value of 330. |
|
Enabled | Appearance | Specifies if the graphic element is available on the HMI device and if the graphic element accepts touch and key input. |
|
Height | Position and Size | Specifies the height in pixels. | Any positive numeric value |
Opacity | Appearance | Specifies the transparency of the graphic element. | 0 (fully transparent) - 100 (fully opaque) |
Visible | Appearance | Specifies if the graphic element is visible on the HMI device. |
|
Width | Position and Size | Specifies the width in pixels. | Any positive number |
X | Position and Size | Specifies the horizontal coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the X property value does not change. | Any positive number |
Y | Position and Size | Specifies the vertical coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the Y property value does not change. | Any positive number |
Provide Feedback