Failed to paste
One of these issues caused the paste operation to fail:
- The component exceeds the maximum allowed components and the paste cannot be completed. For example, the program exceeds the limit of 1000 child programs at the target item, or exceeds the limit of 1000 programs scheduled under a task.
- Another user is making a change to the controller.TheProhibit online edits during uploadcheck box might be selected, which prevents changes to the program when another user is uploading to the controller. This check box appears:
- On theWorkstation Optionsdialog, in theApplicationcategory.
- On theConnected To Uploaddialog when you selectCommunications > Uploadon the main menu or when you selectUploadon theNetwork Browserdialog.
Provide Feedback