Import/Paste Configuration Dialog Box - Configure Programs Overview
Use this dialog to import multiple programs or multiple program hierarchies into a project. The import is executed by selecting multiple programs in the
Controller Organizer
or in the Logical Organizer:- Exporting the programs, selecting a task, and then selecting theImport Componentoption from the File menu, or
- Copying the programs, right-clicking a task in the organizer, and selecting thePaste Special>With Configurationoption from the menu.TIP:ThePaste Special>With Configurationmenu option works when copying from the Controller Organizer to the Logical Organizer, or vice versa.
Imported items are listed in the
Import Content
tree. These items are listed in the Import Content
tree based on what items are part of the import content:- Programs - if you are importing multiple programs, the grid shows the programs that are being imported into the project. If you are importing multiple hierarchies, the grid shows both the programs and the children of the programs that are being imported into the project.
- Tag, Add-On Instruction, Data Type and Other Components - references include any tags directly referenced by any imported logic or tags (via Alias For).
- Connections - lists the Connections from programs that are external to the programs in the import content that are connected to programs in the existing project.
This information describes the settings and information displayed on the
Configure Programs
tab during an import:Setting | Description |
Multiple Programs | The Import Content pane shows the number of programs that are being imported into the project. The value shown in the parenthesis does not include children of the programs. If there are differences among the programs, the difference icon appears in the Differences column of the Programs grid. |
Imported Programs | Shows the number of parent and child programs (if applicable) that are being imported into the project. |
Operation | Identifies what is done with the programs upon import. If Import is selected, all of the programs will be imported into the project. If Discard is selected, none of the programs will be imported into the project. The field is pre-populated with Import . However, you have the option to choose Discard from the pull-down list.
TIP:
To see the
Operation value for a
specific program, access the Programs grid of the program's child
program. |
Schedule In | Shows the task in which all the imported programs are scheduled. The default value for the Scheduled In value is set to either the selected task or Unscheduled Programs/Phases based on which method you use to import the content and from which organizer you initiate the import:
Operation must be set to Import to modify the Scheduled In value. |
Do not change scheduling of existing programs | When this check box is selected, programs that exist in the project remain scheduled as they are configured in the project. The check box is selected by default. When this check box is cleared, upon import, programs are scheduled in the task specified in Schedule In . To modify this option:
|
Parent | Specifies how the programs are organized upon import. When importing from the Controller Organizer, the value of Parent is <none>.When importing from the Logical Organizer:
If Parent is not specified, the programs remain organized as they were configured in the project.Operation must be set to Import to modify the Parent option. |
Do not change parent of existing programs | Select this check box and programs that exist in the project remain organized as they are configured in the project. The check box is selected by default. Clear this check box and upon import, all programs are organized in the program that is specified in Parent . All child programs are imported as organized in the imported content regardless if the check box is selected or cleared. Operation must be set to Import to modify this option. |
Provide Feedback