Change General Logix Designer application preferences
In the
Workstation Options
dialog, use the Application
category to customize
general behaviors in the Logix Designer application. Use the other categories to customize
the behavior for specific editors.To change General Logix Designer application preferences
- From theToolsmenu, clickOptions.
- In theProject Directoryfield, enter the name of the default project directory.
- ClickBrowseto access theBrowse for Folderdialog to search the available directories.
- Select these commands as required:
- Enable Automatic Project Recovery.Periodically saves a temporary copy of the project for recovery after a computer crash or an unexpected shutdown of the Logix Designer application. The recovery file is overwritten with a new recovery file at the save time interval. After a computer crash or unexpected application shutdown, a dialog appears and offers options to save or discard the recovery file.TIP: Certain functions are unavailable in a recovery project, such as toggling a bit or removing forcing.
- Save Time Interval. Enters the interval to save the temporary recovery file.
- Enable Automatic Project Backup.Automatically creates a backup copy of the project while saving the project.Each time the project saves, the Logix Designer application creates a backup of the existing project, and also maintains a backup copy of the old project and a copy of the project with changes. Project backup files are saved in the directory named in theProject Directorybox.Each backup file is named with a .BAKxxx.ACD extension, numbered starting at 000, using this convention:ProjectName.DomainName.UserName.BAK000.ACD
- Number of Backups. Enter the number of backups to keep at one time. The oldest backup file is deleted when the number of backup files is exceeded. For example, if the number of backups is set to 2, when the third backup occurs, file ProjectName.DomainName.UserName.BAK000.ACD is deleted and the Logix Designer application creates backup file ProjectName.DomainName.UserName.BAK002.ACD.
- Enable Look Ahead. Enable automatic selection of an item from a list of typed characters.
- Enable Instruction/Element Defaults. Pre-populate instructions and elements with default values.
- Always Encode Protected Content on Export. Export protected content in encoded format. When clearing the checkbox, if a source key is present, theSaveandExportdialogs enable exporting encoded or plain text.TIP: Use protection permissions to override this selection.
- Use theEnable Large Connection for Downloadcommand to increase the amount of information sent to the controller in a single EtherNet/IP transaction. This setting helps reduce the amount of time required to download networks when using Wifi or a VPN remote connection.Beginning with the Logix Designer application version 31.00, only Ethernet interfaces that support large connections (4,000 bytes) work with these controllers:
- ControlLogix 5590 controllers
- ControlLogix 5580 controllers
- GuardLogix 5580 controllers
- CompactLogix 5380 controllers
- Compact GuardLogix 5380 controllers
- CompactLogix 5370 controller
- Compact GuardLogix 5370 controllers
- 1756-EN2x EtherNet/IP communication modules
- 1756-EN3TR EtherNet/IP communication modules
- 1756-EN4TRx EtherNet/IP communication modules
- Enable Verbose Messaging. Enables detailed messages sent to the message log during project upload and download.By default, the Logix Designer application reduces the time required to upload and download a project by limiting messages to around 20. When you selectEnable Verbose Messaging, additional messages appear in the log, and uploading or downloading a project might take longer.
- Prohibit Online Edits During Upload. Prevents online edits in other instances of the project during project upload.
- Select theHelp page sourcefor Logix Designer Help content:
- Always ask. When you first select aHelpbutton or pressF1in the Logix Designer application, a dialog asks you to select the help source: help files locally installed on the hard drive of the computer running the Logix Designer application, or the latest help content from rockwellautomation.com.Always askis the default setting.
- Local. Displays help files installed on the hard drive of the computer running the Logix Designer application.
- Online. Displays the latest help content from rockwellautomation.com.
If the Logix Designer application cannot connect to rockwellautomation.com, a message states that local help content is displayed. - ClickOKto accept changes and to close theWorkstation Optionsdialog, or clickApplyto apply the changes on this tab and to continue editing.
Provide Feedback