Can't open the specified import file

The specified .L5K file could not be opened. The error message indicates one of these conditions:
Access Denied
Make sure there are read privileges to the file. Check with the Security Administrator to be sure to have access to the file.
File not found
The file does not exist. Enter the name of an existing .L5K file.
Path doesn't exist
Make sure the path exists. If accessing a network drive, make sure there is still a connection to it.
You are trying to import a secured project file from an instance of the
Logix Designer
application that does not have security enabled.
The application must have security enabled and properly configured in order to be able to open secured project files. See the security administrator to have the workstation properly configured, or request a version of the project file that is not secured.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal