Search
FactoryTalk Optix Studio Help Center
Engineering unit converter
BrowseName
EUConverter
SuperType
Converter
(Converter)
Properties
Name
BrowseName
DataType
Description
Raw min
RawMin
Double
Minimum input value to convert.
Raw max
RawMax
Double
Maximum input value to convert.
Scaled min
ScaledMin
Double
Minimum value of the converted unit.
Scaled max
ScaledMax
Double
Maximum value of the converted unit.
Source
Source
Number
Dynamic link mode
Mode
Dynamic link mode
(Inherited from
Converter
)
Is pull
IsPull
Boolean
(Inherited from
Converter
)
Object and variable references
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.