Search
FactoryTalk Optix Studio Help Center
Range
Allows to describe the minimum and maximum value of a variable and to enable the value constraint.
BrowseName
RangeType
SuperType
PropertyType
(PropertyType)
Properties
Name
BrowseName
DataType
Description
Low limit
Low
Double
Low limit
High limit
High
Double
High limit
Constrain
Constrain
Boolean
Enables or disables the constraint on the variable value
Object and variable references
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.