Configure a localization dictionary
Support a multilingual user interface by configuring the appropriate localization dictionaries.
- InProject view, expandTranslations.
- Double-clickLocalizationDictionary1.
- Add the it-IT locale.For more information, see Add a locale language to a localization dictionary.
- Translate strings.For more information, see Translate a string.
Provide Feedback