Module information

In the ControlLogix chassis figure, the location of the Historian module in the chassis slot is marked with green, while the location of the controller with grey.
The
Module Information
section displays the following information:This item | Displays |
|---|---|
Name | The name of the module. |
Firmware Version | The version of the firmware. |
Current Time | The current time of the module. |
Up Time | The total time the module has been running. |
Provide Feedback