Module information

Module information (2)
The
Module Information
section displays the following information:
This item
Displays
Name
The name of the module.
To change your module name, click the
Advanced
tab, and then click
System Settings
.
For details on the module name and information on the impact of changing the module name, see Change the module name.
Firmware Version
The version of the firmware.
Current Time
The current time of the module.
To configure time settings, click the
Advanced
tab, and then click
Time Management
.
Up Time
The total time the module has been running.
Module Slot Location
The location of the module in a slot in the ControlLogix chassis.
Serial Number
The serial number of the module.
This number cannot be changed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal