Client connections

Client connections
The
Client Connections
section displays the number of clients currently connected to FactoryTalk Historian ME. There may be up to 5 clients connected simultaneously to the Historian module.
The following client applications are supported:
  • FactoryTalk Historian DataLink
  • FactoryTalk Historian ProcessBook
  • FactoryTalk View SE Trending
  • FactoryTalk Administration Console
  • PI System Management Tools (SMT)
  • FactoryTalk VantagePoint
  • FactoryTalk VantagePoint EMI
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal