Edit point discovery rule files
To edit a point discovery rule file
- In theFactoryTalk Historian ME Rule Editorwindow, clickRule File Management.TheFactoryTalk Historian ME User Defined Rule File Listdialog box appears.
- Select the rule file that you want to edit, and then clickOpen.The rule file appears in theFactoryTalk Historian ME Rule Editorwindow.The rules defined in the file appear in the table.
- Make your changes to the rule file:
- To change the file description, type a new one in theDescriptionbox.
- To add a rule, clickNew.For details, see Define point discovery rules.
- To edit a rule, select the rule, and then clickEdit.For details, see Define point discovery rules.
- To remove a rule, select the rule, and then clickDelete.In the message box that appears, clickYes.
- ClickSave.
Provide Feedback