Time management issues
Symptom | Solution |
|---|---|
You have forgotten the module's time synchronization source. | Go to Web Diagnostics , and under the Hardware tab check the Time
Management page. The time source is listed in the Time Source
section. |
The module is synchronized to a controller time source and the controller time is moving back, causing the module time to move back. |
|
The module is synchronized to an NTP time source, and the module time is incorrect. |
|
The module starts in safe mode after a restart because the user accidentally typed a past time when configuring the module time. |
|
Provide Feedback