View data transfer statistics
The data transfer service records performance statistics that determine the connection reliability. You can use the statistics to refine the data transfer configuration.
The
Data Transfer Statistics
section of the page displays the following information:Item | Description |
|---|---|
Transfer Rate | The number of retrieved events divided by the number of minutes spent on retrieving events sent to the FactoryTalk Historian SE or PI server. |
Successful Attempt Rate | The number of attempts to transfer data to the FactoryTalk Historian SE or PI server per hour. |
Provide Feedback