FactoryTalk licensing

FactoryTalk Historian ME
limits the clients that can access it. Client connections are limited to
Rockwell Automation
preferred clients. This means that no anonymous connections will be accepted. The following applications can access
FactoryTalk Historian ME
:
  • FactoryTalk® Historian DataLink
  • FactoryTalk®
    Historian ProcessBook
  • FactoryTalk® View Site Edition (SE)
    Trending
  • FactoryTalk® Administration Console
  • PI System Management Tools (SMT)
  • PI SMT Tag Configurator and PI Builder
  • FactoryTalk® VantagePoint®
    and FactoryTalk VantagePoint EMI
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal