Create SNMP community strings
Create SNMP community strings to use them as passwords to enable access to a device's
statistics.
TIP:
- Only accounts with piadmin or FTHAdministrators privileges can modify the contents ofSNMP Managementpage.
- While SNMP is enabled, it is not possible to add or delete community strings.
- The string can contain up to 35 alphanumeric characters (A-Z, a-z, 0-9).
- FactoryTalk Historian ME supports a maximum of 5 community strings.
To create SNMP community strings
- Select theAdvancedtab, then selectSNMP Management.
- Uncheck theEnable SNMPcheckbox.
- SelectCreate.
- In the next screen, enter the community string.
- SelectSave.
- Repeat steps 3-5 as needed.
- Re-check theEnable SNMPcheckbox.
Provide Feedback