Integrate the module into a FactoryTalk environment with the FactoryTalk Directory

In this section, you will learn how to integrate a standalone
FactoryTalk Historian ME
module into an existing FactoryTalk system using the
FactoryTalk Directory
. Integrating a standalone module into an existing FactoryTalk system allows:
  • Centralized administration of security credentials, performed in the
    FactoryTalk Administration Console
    .
  • FactoryTalk clients (for example, FactoryTalk View SE or FactoryTalk Batch) to connect to the
    FactoryTalk Historian ME
    module.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal