Create shortcuts to the local chassis
When creating local shortcuts, take into consideration the following points:
- You can create up to 5 shortcuts to the local chassis.
- The shortcut paths must be unique. This means that each shortcut must point to a different controller or have a different CIP path.
- If you create a shortcut to a controller which is used for time synchronization, the time will no longer be synchronized with this controller after you save your changes.This is because adding a shortcut to a controller changes the name structure of the tags from the controller, which means previously defined tags will be disabled. For details, see Tag naming conventions.
- If you create a shortcut to a controller which is used for collecting data, the data will no longer be collected from this controller after you save your changes.This is because adding a shortcut to a controller changes the name structure of the tags from the controller, which means previously defined tags will be disabled. For details, see Tag naming conventions.
- Creating shortcuts to local controllers is optional.
To create a shortcut to the local chassis
- ClickManage Points, and then clickManage Shortcuts.
- ClickAdd.
- Select the controller to which you want to create a shortcut.Alternatively, select theAdd the shortcut using a CIP path insteadoption, and type the CIP path to the controller.
- Type the name of the shortcut.When typing the name, take into consideration the following points:
- The name can contain only the characters a-z, A-Z, 0-9, and an underscore.TIP:To learn about the convention of naming tags added to the Historian module using the shortcuts, see Tag naming conventions.
- The maximum length of the name is 40 characters.TIP:To minimize the complexity of tag names, we recommend that you keep the shortcut names short.
- The name must start with a letter or an underscore.
- The name cannot contain two underscores side by side, or an underscore with a number at the end of the name (for example, shortcut_12).
- The shortcut name must be unique.
- ClickSave.The shortcut is added to the shortcut table.TIP:If any error occurs when creating the shortcut, it is indicated with a message displayed at the top of the page.
Provide Feedback