Install FactoryTalk Historian ME Logix Designer Module Profile

FactoryTalk Historian ME
can be configured to communicate with a ControlLogix controller through the
FactoryTalk Historian ME
Logix Designer Module Profile.
TIP:
Install the Module Profile on the computer with
RSLogix 5000®
or Studio 5000 installed.
To install the Module Profile
  1. Run the
    FactoryTalk Historian ME
    Client Tools DVD.
    The installation wizard appears.
  2. Click
    Install
    FactoryTalk Historian ME
    Client Tools
    >
    Install
    FactoryTalk Historian ME
    Logix Designer Module Profile
    .
    The Logix Designer Module Profile installation wizard appears.
  3. Follow the on-screen instructions to complete the process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal