(optional) Install ControlFLASH or ControlFLASH Plus

Starting from ControlFLASH version 13.00, when the installation completes, FactoryTalk Security is enabled by default. When launched, ControlFLASH logs on to the FactoryTalk Network Directory.
TIP:
For details on using ControlFLASH or ControlFLASH Plus, see its documentation.
To install ControlFLASH or ControlFLASH Plus
  1. Extract the installation package and double-click
    Setup.exe
    .
    The Rockwell Automation Installer appears.
  2. Follow the instructions to complete the installation process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal