Add the module website to the Local intranet security zone

To add the module website to the Local intranet zone
  1. Open the FactoryTalk Historian ME website using the IP address of the module.
  2. On the
    Tools
    menu, click
    Internet Options
    .
    The
    Internet Options
    dialog box appears.
    TIP:
    If the top menu is not visible, press the left Alt key on your keyboard to bring up the top menu.
  3. Click the
    Security
    tab, and then select
    Local intranet
    .
    Add the module website to the Local intranet security zone (2)
  4. Click
    Sites
    .
    The
    Local intranet
    dialog box appears.
  5. Click
    Advanced
    .
    The
    Local intranet
    dialog box appears.
  6. Verify that in the
    Add this website to the zone
    text box there is a URL of your module site, and then click
    Add
    .
    The URL of the module website appears in the
    Websites
    list. Depending on the security protocol used to communicate with the module, the website URL will be prepended by
    https
    prefix. You need to add the URL, starting with
    https
    prefix, to the
    Websites
    list.
  7. In the
    Add this website to the zone
    text box, type the IP address of the module with the prefix other than the one of the URL already added to the
    Websites
    list, and then click
    Add
    .
    Both URLs for the module website appear in the
    Websites
    list.
  8. Click
    Close
    , and then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal